Issue:
Communications cable to use between the Twido mini din and Magelis HMISTU655/855 RJ45 port
Product Line:
Twido, HMISTU
Resolution:
The communications cable between the Twido PLC and the HMISTU655/855 is the XBTZ9780.
Опубликовано для:Schneider Electric Казахстан