Issue
Need to reset the Circuit Monitor Series 2000 back to the factory default settings.
Product Line
CM2000 Series
Environment
Programming
Resolution
This should always be the last resort.
Reseting the meter will clear the CT/PT ratios, System Type, I/O setup, Alarms/Events, Data Logs, Event logs, Waveform Capture Logs, and etc.
The device address and baud rate are not reset on versions 14.000 or later.
The attached article explains how to reset the CM2000 to factory default
Опубликовано для: Schneider Electric Казахстан