{}

Buscar Preguntas Frecuentes

{"searchBar":{"inputPlaceholder":"Busca por palabra clave o haz una pregunta","searchBtn":"Buscar","error":"Ingresa una palabra para buscar"}}

I need an electromechanical relay, and my output is higher than 28 VDC, what relay series should I look at?

Issue:
When selecting an electromechanical relay that is more than 28 V DC, need suggestions

Product Line:
General Purpose Relays

Environment:
General Purpose Relays

Cause:
Product selection

Resolution

When selecting an electromechanical relay for an application with an output higher than 28 volts DC, a magnetic blowout would be needed. If the voltage is higher than 28 volts DC the current will be de-rated as well.
  • The 750, 788, and 199 relay series include parts with blow out magnets.
  • The 750 & 788 relay series designates code "69" for a blowout magnet.
  • The 199 relay series designates code "B" for a blowout magnet.

¿Te fue de ayuda?