Browse FAQs

Is the XB3 or ZB3, 30mm pushbutton line still available?

Published date: 07 August 2020

Issue:
XB3 and ZB3, 30mm operators

Product Line:
30mm Push Buttons

Environment:
30mm Telemecanique 30mm Operators

Resolution:                                                                 
The XB3 product is no longer available. It used the same contact blocks, light modules, and lenses as the XB2 line.  So some parts are still available.
Recommend to replace the complete device with the 9001 Type K (metal) or 9001 Type SK (plastic) line.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.