Browse FAQs

Is the remote keypad option available for Altivar 21 Drive.

Published date: 08 September 2019

Yes, the remote keypad option is available for the Altivar 21 Drive. The reference for the same is VW3A21101. It can be installed remotely up to a distance of 5 meters maximum.

Refer to attached document for the kit part reference, Kit contents and Functional Instructions.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.