Browse FAQs

How do you change the port parameters of the Modbus configuration (CFG) port of an Advantys STB network interface module (NIM) ?

Published date: 28 August 2019

Goals and Symptoms

How do you change the port parameters of the Modbus configuration (CFG) port of an Advantys STB network interface module (NIM)

Facts and Changes

Advantys Configuration Software

Causes and Fixes

This would be an online function utilizing the Advantys Configuration software. First, connect to the NIM with the Advantys Configuration software via the MB (CFG) port or Ethernet port in the case of the STBNIP2212. Once connected, go to the Online menu and select Configuration Port Settings. Now you can modify the port settings including Modbus Node ID, Baud Rate, and other communication parameters. Selecting OK will then prompt you that you will be disconnected and need to confirm. Once confirmed, you will be disconnected and your new port settings will be established. Now you can reconnect to the MB (CFG) port via the new port settings.


Legacy KB System (APS) Data: RESL198144 V1.0, Originally authored by DaSo on 03/27/2009, Last Edited by DaSo on 03/27/2009
Related ranges: Advantys STB

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.