Browse FAQs

Will the ProWORX NxT run on Windows 7 Operating Systems?

Published date: 06 September 2019

Issue:
Will Proworx NxT programming software run on a Windows 7 operating system?

Product line:
All products that run on Proworx NxT software.

Environment:
Proworx NxT

Cause:
Software will not run on Windows 7

Resolution:
ProWORX NxT is not qualified to run on Windows 7.
The ProWORX NxT authorization will not run properly on the Windows 7 O.S. NxT is a 16-bit program. Windows 7 is either a 32 or 64-bit application.
ProWORX NxT will not be qualified to run on Windows 7. You will need to upgrade to ProWORX 32 v2.1 SP2, which is qualified to run on the Windows 7 Pro 32 or 64-bit platforms.

NOTE: Proworx software is now obsolete.  Check with service.sales@schneider-electric.com for availability.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.