Browse FAQs

Is it possible to rename a DFB in Control Expert (formerly Unity Pro.) ?

Published date: 28 August 2019

Yes it is possible to remname the DFB by following the steps below.

Go to Derived FB Types and right click on the DFB that you want to rename.
<Export.>
Assign a name. DFBname.XDB, for example.

Right click on Derived FB Types and <Import>.
Confirm. <Yes>.
Choose DFBname.XDB.
Highlight the line that calls out the DFB.
Double click on the ' X' in the Rename column.
Rename as: Newdfbname. <Rename> <OK>.

You can then edit this DFB and/or delete the original DFB.


Legacy KB System (APS) Data: RESL210438 V1.0, Originally authored by DaSo on 01/28/2013, Last Edited by DaSo on 01/28/2013
Related ranges: Unity Pro - SoCollaborative software

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.