Browse FAQs

How may the Zone Selective Interlocking (ZSI) contacts be modified on a Sepam 80 series relay?

Published date: 06 September 2019

Issue
Need to modify the ZSI contacts

Product Line
Sepam 80 Series Relays

Environment
SFT2841 Software

Resolution
The ZSI contacts are configured in the Control Matrix within SFT2841. To modify the contacts associated with ZSI navigate to the Control Matrix then click on Logic > Outputs. This will allow you to change the contacts associated with any of the Sepam Relays predefined logic.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.