Browse FAQs

What is the description for part number 3042653253?

Published date: 04 August 2020

Issue:
What is a 3042653253?

Product Line:
Push Buttons and Operator Interface

Environment:
9001 control stations

Cause:
Non standard replacement part

Resolution:
3042653253 is a toggle switch in a Type NEMA 7 and Type NEMA 9, Class 9001B control station. 
These control stations were obsoleted in 1994 along with all component parts.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.