Browse FAQs

What is the minimum voltage value of DC bus for ATV61...N4?

Published date: 27 July 2020

Issue:
Under supply minimum voltage value.

Product Line:
Altivar 61

Environment:
ATV61...N4 - 380v version

Cause:
None

Resolution:
For ATV61..N4 (380V), the minimum value of DC bus you have to overcome at least 430VDC (304VAC), then you can go even below USFLmin (268VDC-190VAC in case of 380VAC), this value can be adjusted from USL parameter.
Below you will find the page for the values
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.