Browse FAQs

How do you set up the ATV312 drive for modbus control?

Published date: 11 September 2019

Issue:
Setting up the ATV312 drive for modbus control.

Product Line:
Altivar ATV31 ATV312 drives

Environment:
All

Cause:
Needs to set up the ATV312 drive to do modbus control over the network.

Resolution:
Programming
1st set up your modbus address in the CON menu
Add= modbus address enter 1 thru 247
tbr= modbus baud rate 4.8K thru 19.2K
tFo= modbus format: 8-O-1, 8-E-1, 8-N-1 or 8-N-2
tto=modbus time out 0.1 thru 30 seconds

2nd set up your ref and command channel in CLT menu
LAC= Level 3  hold enter in for 3 seconds
FR1= modbus

Important addresses
Command address
8501= CMD address for start and stopping
8502= LFRD speed ref in hz  0.1hz  example 600 value equals 60hz

3201= ETA address for status
3202= output speed in hz 0.1hz  example 600 value equals 60hz

Pinouts
Pin 4=D1 modbus
Pin 5=D0 modbus
Pin 8= Common for modbus

See the attached documents for more programming and modbus information.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.