Browse FAQs

Osisense XC_Obsolete XCKP9279 switch with reset : how to replace it

Published date: 16 December 2020

The obsolete XCKP9279 switch was a roller lever plunger switch with 2 NC contacts, snap action block, for vertical direction (special model), having reset function, plastic casing in black colour. The equivalent switch in the Osisense XC offer is the XCPR2927G13 commercial reference with 2NC contacts positive opening, snap action. Attached corresponding datasheet downloaded from "tesensors.com" site.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.