Browse FAQs

Why doesn't my Biometric Switch run on my Windows 7 / Windows10 64-bit OS?

Published date: 31 July 2020

Issue:
Unable to use a Harmony XB5S Biometric Switch on a Windows 64-bit OS.

Product Line:
Harmony XB5S, Mageils iPC (64-bit OS), Vijeo Designer Runtime (all versions)

Resolution:
Depending on your Windows User Account Control (UAC) settings, you may need to run Vijeo Designer Runtime as Administrator before the Biometric switch will initialize properly.

To do so, right click on the Vijeo Designer Runtime Icon and select "Run as Administrator".

Alternatively, enable the "Run as Administrator" in Compatibility tab of the Shortcut

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.