Browse FAQs

How to adjust the screen brightness on XBTGT7340

Published date: 23 August 2019

Issue:
Looking for a way to change the brightness levels of the LCD screen of the XBTGT7340.

Product Line:
Magelis, HMI, XBTGT, HMIGK, HMIGTO, HMIGTU, HMISTO, HMISTU, XBTGK, XBTGH

Resolution:
To adjust the screen brightness of the XBTGT7340, a touch script can be made as follows:

You could write the following in a switch script to increment: _Brightness.write(_Brightness.getIntValue() + 1); and then this to decrement: _Brightness.write(_Brightness.getIntValue() - 1);

Alternatively, there are toolchest parts that you could drag on the panel that allow you to adjust the brightness as well.

Finally, you could also adjust the brightness from the HMI's configuraiton menu.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.