Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
M580 and cat6 cable
Issue
Can a cat6 redundancy capacity used with M580?
Product Line
M580, M340
Resolution
The M580 processors do not use the second pair of Ethernet lines present on a Cat6 cable. Using the redundant pairs in a cat6 cable between two networks was not tested/qualified on none of our equipment, so it is not supported.
Can a cat6 redundancy capacity used with M580?
Product Line
M580, M340
Resolution
The M580 processors do not use the second pair of Ethernet lines present on a Cat6 cable. Using the redundant pairs in a cat6 cable between two networks was not tested/qualified on none of our equipment, so it is not supported.
Published for:Schneider Electric Malaysia
Did this answer your question?
Explore more
Explore more