Browse FAQs

How to reset peak demand from the front display of a CM4000

Published date: 04 September 2019

Product Line
CM4000 series

Environment
Keys on the front display.

Resolution

To reset the demand peak values, follow the procedure below:

  1. From the Front Panel Main Menu, select Resets
  2. Select Demand. The password prompt displays.
  3. Select your password. The default password is 0.
  4. The Reset Demand Screen displays. Select the value that you need to reset. Available options are Peak Power Demand and Peak AMP Demand.
  5. Press Enter on the selected option. The "No" option starts to blink
  6. Use the Up arrow to change to "Yes", then press Enter. The Yes will stop blinking
  7. Press the Menu button. You will get a confirmation that the Reset was complete. 
  8. Press the Menu button two more times to return to the Main Menu Screen.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.