Browse FAQs

Does Schneider Electric offer the servo motor type BMH1002S0015 ?

Published date: 04 September 2019

No, the BMH motor with model BMH1002S0015 is a special version for the company W & H and is a proprietary product which is not available directly from Schneider Electric.
This motor has a special version of winding for the OEM machine and is not replaceable with a standard version.
Customers looking for BMH1002S0015 must contact the OEM machine builder W & H, for a spare motor of this type.



rev 9-4-19

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.