Browse FAQs

What is the power dissipation for the XBTGT7340?

Published date: 20 August 2019

Issue:
Looking for information regarding the power dissipation for the XBTGT7340 series of HMI.

Product Line:
Magelis XBTGT7340

Resolution:
The power dissipation of the XBTGT7340 is max. 35.3W (with 12W external load).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.