Browse FAQs

ATV61 - Cannot change the default display from Hertz to percentage

Published date: 04 August 2020

Issue:
Parameters changed are reverting back to default

Product line:
All Altivar drives and Altistart soft starters.

Environment:
All models, All serial numbers.

Cause:
Programming changes to my drive are being lost, and the parameters return to the previous settings.

Resolution:
If a run command is present, or if the drive is in freewheel mode (NST), programming changes can not be made on the drive for most parameter.   Be certain that the drive state is ready (RDY) before making programming changes to the drive.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.