Browse FAQs

What is the part number for an E-Flex fan wire extender?

Published date: 04 August 2020

 Issue:
Part number for an E-Flex fan wire extender
 
Product Line:
E-Flex
 
Environment:
All models
 
Cause:
Damaged wire needs replaced.
 
Resolution:
These wires extend the heatsink cooling fan leads to reach the VFD plug receptacle.  The extender wires are only available as a component to the flange kit used to assemble the E-Flex.  Flange kits are VW3A95** based on the VFD model.  Search FAQ with keywords: ATV61 flange kit.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.