Browse FAQs

How is the 50C rating accomplished in the Enclosed ATS22 Soft Start Controllers?

Published date: 17 August 2020

Issue:
Customer ordered an Enclosed Altistart 22 and there is no circulating fan inside the enclosure.

Product line:
Enclosed ATS22, Altistart 22

Environment:
NEMA 1 and NEMA 12 enclosed. 

Cause:
Customer has ordered but found no circulating fan inside.

Resolution:
Engineering uses an oversized ATS22 softstart with de-rating based on temperature instead of adding a cooling fan.

Example: 
ATS22C14S6U has 124 nominal motor current. We want 52C rating, so over nominal temperature (40C) by 12C. 
We have a derating of 2.2% for every 1C over 40C.
52-40= 12.  
12x2.2% = 26.4%. 
26.4% of 124 = 32.24.  
32.24 is the deduction for the 124 nominal motor current of ATS22C14S6U. So the ATS22C14S6U has only rated to 91.76A motor in 52C temperature. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.