Browse FAQs

Can you connect multiple ATV320 drives to one keypad?

Published date: 11 August 2020

Issue:
Wants to have a cabinet with multiple Altivar 320 drives, but only use one keypad on the door to access each.

Product line:
Altivar Machine, Altivar 320

Environment:
Altivar 320

Cause:
Application for OEM
Multiple drives

Resolution:
Yes, you can connect multiple drives with one keypad.  See the attached catalog page from the ATV320 catalog for details.
Schneider has used up to 10 drives with one keypad.  More than 10 drives has not been tested.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.