Browse FAQs

What is the response time of the TM3XTRA1 and TM3XREC1?

Published date: 26 August 2019

Issue
What is the response time between the TM3XTRA1 and TM3XREC1 transmitter and receiver modules for extended I/O?

Product Line
Modicon TM3 Expansion I/O modules for M221, M241, M251, M262 PLCs

Environment
Performance of Physical PLCs and Input/Output modules

Resolution
The response time between the TM3XTRA1 and TM3XREC1 transmitter and receiver modules for extended I/O depends on the size of the data on all the TM3 bus, but can be guaranteed to be less than 5 milliseconds in all cases.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.