Browse FAQs

How does the XPSECME5131P replace the XPSECM5131 when they are different sizes?

Published date: 25 August 2020

Issue:
XPSEMCE wiring to replace XPSECM5131 or XPSECP5131

Product line:
XPSEMCE5131P

Environment:
Machine Safety

Cause:
XPSECM is obsolete

Resolution:
See the attached comparison in the two wiring diagrams.  The XPSECM is obsolete so the customer can only use the new expansion modules.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.