{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Does the ATS48 come with the shorting contactor as a standard component when it is ordered?
Issue:
Wondering if the ATS48 comes with the shorting contactor, as a standard component when it is ordered?

Product Line:
ATS48

Environment:
Shorting contactor

Cause:
n/a

Resolution:
No. It can be ordered as a separate component to be added in the field.

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: