{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can the display be set to show a specific parameter as the default the Altistart 48?
Issue:
Set display to show specific parameters as the default the ATS48.

Product Line:
Altistart 48

Environment:
All

Cause:
Display customization

Resolution:
The factory setting displays the motor current (parameter LCr).
To save the chosen display:
You must make these changes from the keypad on the face of the starter itself.  These changes can not be made via the remote keypad, if present.
- Press the ENT key once: the choice is temporary, it will be cleared at the next power up.
- Press the ENT key again for 2 seconds: the display flashes, the choice is permanent and will be retained even if power is cycled.

The available display parameters are:
COS - power factor
LCr - Line current
rnt - hours of run time
LPr - Line power in terms of percentage nominal
Ltr - motor torque in terms of percentage nominal
LAP - Power in terms of kW
EtA - Soft Starter status (rdy, acc, dec, run etc.)
LFt - Last fault detected
PHF - Phase rotation
COd - keypad locking code

Schneider Electric Nigeria