{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
When does the INF3 (Internal Serial Link) fault occur in Altivar 61/71 Drive.

The Internal Serial Link Fault (INF3) occurs in Altivar 61/71 Drives when the 24VDC internal power supply is disturbed, causing the reset of microprocessor. The second likely reason is that the communication between the internal boards i.e. Power board, Motor Control board and Application Board is disrupted.

To remove the fault, check the internal connections, tightness of ribbon cable & connectors of internal boards. Also ensure that the power cable and the control cable are separated in the external wiring. Lastly replace the Motor Control Board or the Terminal Board.

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: