{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Single Phase Symmetra Extended Run (XR) Frame Cable Lengths

Issue:
What are the lengths of the DC cables that are attached to single phase Symmetra extended run (XR) frames?

Product Line:
Single Phase Symmetra XR Frames

Environment:
All serial ranges

Cause:
These products are designed to be able to reach each other if position in the same area.  This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example.

Resolution:
The following table outlines the cable lengths of the DC cable provided with each of the single-phase Symmetra Extended Run cabinets.

XR Type

Cable Type and Length

SYXR4

Fixed or Detachable 5ft (1.5m)
SYXR12

Fixed or Detachable 5ft (1.5m)

SYRMXR4

Fixed 2ft (0.6m)

SYARMXR3

Fixed 3.5ft (1.0m)

SYARMXR9

Fixed 5ft (1.5m)

SYAXR9

Fixed 5ft (1.5m)




Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: