{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
DIN Connector Pin Outs For the Netbotz Appliances
Issue:
DIN Connector Pin Outs For the Netbotz Appliances

Product Line:
NetBotz

Environment:
NetBotz version 1 and 2 cables

Cause:
Pin-out specifications.

Resolution:
DIN Connector Pin Outs

-NetBotz does not release the pin outs for the DIN connectors for any NetBotz Appliances.

-To address this issue, NetBotz sells a standard dry contact cable that is our DIN connector one end and two bare dry contact style wires on the other.

-This cable is provided to allow customers to attach our NetBotz Appliances to any dry contact type connection without having to have the DIN connector pin outs.




Schneider Electric Nigeria