{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can the APC NetShelter SX or SV cabinet be disassembled to accommodate moving through a narrow doorway?
Issue:
The NetShelter SX cabinet needs to be disassembled.
Product Line:
NetShelter SX, SV
Environment:
All versions and serial ranges.
Cause:
Small doorways, stairs or elevator may force the need for the cabinet to be disassembled.
Resolution :

NetShelter SX cabinets are not made to be disassembled. Doing so will void the warrantee and the UL mark.
If a NetShelter SX cabinet needs to move through a small doorway, and must disassembled, please contact your local APC by Schneider Electric Customer Care Center for instructions. You may want to consider using the NetShelter SV AR2400FP1. This is a flat-packed (unassembled) cabinet that's designed to be assembled on site.

NetShelter SV cabinets are not made to be disassembled, with the exception of AR2400FP1. Doing so will void the warrantee and the UL mark.
If a NetShelter SV cabinet needs to move through a small doorway, and must disassembled, please use the Owner's Manual for AR2400FP1 to do so. The Owner's Manual is available on the NetShelter SV section of the APC website, under the Documentation tab.

Note: if a NetShelter SX or SV cabinet is disassembled, for re-assembly the cabinet needs to be on the most level surface possible to assure squareness.

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: