{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the input voltage required for the InRow ACRD100/200? Is a power cord supplied with the unit?
Issue:
The article addresses the question of, what is the input voltage required for the InRow ACRD100/200? Is a power cord supplied with the unit?

Product line:
ACRD100.

Environment:
All versions.

Cause:
Install.

Resolution:
The InRow RD unit uses a single phase 208V/60Hz input in NAM and a 230V/50Hz input in the rest of the world. Is a power cord supplied with the unit?   No

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: