Search FAQs
How do you set up a end of damper for the legacy ATV212 S-Flex enclosed drive?
Issue:
End of damper control for a S-flex ATV212 with bypass option.
Product Line:
Altivar
Environment:
Altivar Machine
Cause:
Set up Damper control
Resolution:
End customers auto start will need to start up Damper Solenoid. Once the Damper is open you will need a damper relay to close (R) to indicate damper is in correct position.
You will need qty 3 end of damper dry contacts.
wire you 3 end of damper dry contacts to:
P24 to R
Terminals 2 to 4
add dry contact in series with R input on the drive.
see the attachment for example diagram.
End of damper control for a S-flex ATV212 with bypass option.
Product Line:
Altivar
Environment:
Altivar Machine
Cause:
Set up Damper control
Resolution:
End customers auto start will need to start up Damper Solenoid. Once the Damper is open you will need a damper relay to close (R) to indicate damper is in correct position.
You will need qty 3 end of damper dry contacts.
wire you 3 end of damper dry contacts to:
P24 to R
Terminals 2 to 4
add dry contact in series with R input on the drive.
see the attachment for example diagram.
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: