{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I invert the mA analog input signal on an E-Flex Altivar 61?
Issue:
mA signal inversion so the drive runs at low speed at 20mA and high speed at 4mA

Product line:
Altivar ATV61, ATV71

Environment:
All models, all serial numbers

Cause:
Inverting the mA analog input signal

Resolution:
Menu 1.5 AI2 configuration AI2 min set to 20mA and AI2 max set to 4mA
ATV71_programming_manual ref

Schneider Electric Nigeria