{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
VMware Tools status displays as "Out-of-date" after deploying the PowerChute Network Shutdown Virtual Appliance.
Issue:
After you install PowerChute Network Shutdown by deploying the virtual appliance, VMware Tools shows an "Out-of-date" status.

Product Line:
PowerChute Network Shutdown v3.1 - v4.2

Environment:
VMware

Cause:
The PowerChute Network Shutdown virtual appliance was created on ESXi. When deploying the OVA file to a later version of ESXi, the VMware Tools status displays the "Out-of-date" status.

Resolution:

Right-click on the PowerChute Network Shutdown appliance in vSphere Client.
Choose Guest - Install/Upgrade VMware Tools.
Choose Automatic Tools Upgrade.

This will update the version of VMware Tools to the latest version in order to match the version of the ESXi host you have deployed on.

NOTE: This issue is resolved in the CentOS 7 based PowerChute Network Shutdown v4.3 virtual appliance.

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: