undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Why do I get SIZE ERR 4K on my 8005PR4 when I try to write the program to my SY/MAX model 50 memory pack?

Issue

Why do I get SIZE ERR 4K on my 8005PR4 when I try to write the program to my SY/MAX model 50 memory pack?

Product Line

SY/MAX

Environment

8005PR4

Resolution

"SIZE ERR 4K" is displayed on the 8005PR4 when an attempt is made to write a 4K step program to a 1k-step memory pack. To overcome this the user must replace the 1K-step memory pack (8005MP1) with a 4K-step memory pack. There are three models of 4K-step memory packs: 8005MP4 (CMOS-RAM with battery), 8005MP14 (EPROM) and 8005MP24 (EEPROM).

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: