undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between the 8020SCP423 and 8020SCP424 SY/MAX controllers?

Issue

What is the difference between the 8020SCP423 and 8020SCP424 SY/MAX controllers?

Product Line

SY/MAX

Environment

8020SCP423

Resolution

The only difference between the 8020SCP423 and 8020SCP424 SY/MAX controllers is the size of their user memory. The 8020SCP423 has 8K of RAM. The 8020SCP424 has 16K of RAM.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.