undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the diameter of the Lexium high power cables AGOKIT019MXXX?

Issue
What is the diameter of the Lexium high power cable AGOKIT019MXXX?

Product line
Lexium BPH

Environment
AGOKIT019MXXX

Resolution
The diameter of the AGOKIT019MXXX cables is 15.5mm

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.