undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
STBAVO1250 Byte Reversal in a Profibus Island Fixed in Exec v2.02

Issue

If a Profibus master and STBNDP2212 island were power cycled simultaneously, when communication resumed, the output channel upper and lower bytes sent to an STBAVO1250 would occasionally be swapped. After the described power cycle was done, 3200 Hex sent to the Profibus island could result in 0032 Hex being written to an AVO output channel register. Another power cycle cleared the error and resulted in the bytes being written correctly.

Product Line

Advantys, STB

Resolution

The issue has been addressed with new executive software for the STBNDP2212. Those NIMs loaded with v2.02 executive software will not display the problem.
Production modules loaded with the exec are marked SV: 02.02 and PV:08.

The web accessed exec file name is ai_nim_ndp_02_02.bin.

The problem had been observed when a Siemens S7315-2DP w/2.00 firmware was used for the head. Other head configurations had not been observed to cause the problem. However, due to the intermittent nature of the problem, users were cautioned to not power cycle Profibus heads and associated STB islands at the same time.

This resolution replaces an earlier version that described the problem and indicated a fix was being investigated.


Legacy KB System (APS) Data: RESL172489 V3.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: