{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Quantum CPUx13 EXEC rev 2.43 and 2.44 use wrong time base

Goals and Symptoms

The EXECs rev 2.43 and 2.44 for the Quantum CPU 113 02 / CPU 113 03 / CPU 213 04 (q186v243.bin, q186v244.bin)

    • and CPU 113 02S /CPU113 03S / CPU 213 04S (q1sv243E.bin and q1sv244E.bin) use a wrong time base.
      The time base is about 20% too fast.

Facts and Changes

The bug results in wrong time behavior of:
- System functions like Online PLC scan time and the application watch dog timer.
- All time dependent IEC-EFBs like TON, TOF, FREERUN, SYSCLOCK etc.
- All time dependent LL984-Instructions like T.01, T0.1, T1.0, PCFL etc.

The internal RTU time (Time of Day clock) is not affected.

Previous Concept 2.6 SR4 (PN:33002308.07) contained the EXEC version 2.43.
Meanwhile the Concept V2.6 SR 4 CD has been updated. PV08/RL08 contains EXEC rev 2.45
Patch B for Concept 2.6 SR4 contains the EXEC version 2.44.
Patch C for Concept 2.6 SR4 contains the EXEC version 2.45.

Causes and Fixes

Use EXEC rev 2.45 (q186v245.bin or q1sv245E.bin) or higher EXEC s also are available on www.telemecanique.com

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: