{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to protect the ConnexView network file after it is discovered and adjusted.

Issue
How to protect the network file after it is discovered and adjusted with ConnexView.

Product Line
Connexium Network Maager

Environment
Windows 7

Resolution
Changes to the 'ConnexView' network discovery file can be prevented by write protecting it.

This can be performed by:

  • Locate the network file in the 'C:\Program Files\Schneider Electric\ConneXview\networks.' folder
  • Right Click on the filename.
  • Select 'Properties'.
  • Change the attributes in the 'General' tab to 'Read only' by selecting the checkbox.
  • Click on 'OK' to close the window.


Note: The user can still change the network in 'ConnexView' but they will not be able to save the changes.
An 'unable to save network' message will appear when they try to save it.

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: