{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the din rail mounting kit part number for the ATV312?
Issue:
Part number for ATV312 Din rail mounting kit

Product Line:
ATV312

Environment:
All

Cause:
Desire to utilize din mounting kit option

Resolution:
The part numbers need to order the mounting kit for this drive are VW3A9804 and VW3A9805.

VW3A9804 covers the following range of drives: ATV312....
018M2, H037M2, H055M2, H075M2, H018M3, H037M3, H055M3, H075M3

VW3A9805 covers the following range of drives: ATV312....
HU11M2, HU15M2, HU11M3, HU15M3, HU22M3, H037N4, H055N4, H075N4, HU11N4, HU15N4, H075S6, HU15S6
Note: The din rail mounting kits are only available for the above drives.

Note: Other drives not list above do not have a din rail kit.

Schneider Electric Nigeria