undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the state of the ATS48 Fault relay for various conditions?

Article available in these languages: Spanish

Issue:
State of the ATS48 Fault relay contact for the following conditions

Product Line:
Altistart ATS48

Environment:
All models

Cause:
None

Resolution:
Relay R1 functions as a fault relay on terminals R1A-R1C when Menu IO, parameter r1 = r1F.
It is a normally open contact.

Conditions:
Control power not applied to CL1-CL2,  contact is OPEN
Control power applied and no fault,  contact is CLOSED
ATS48  detects a fault,  contact is OPEN

Note special case where Automatic Restart is active, Menu PrO, parameter ArS = ON.  When an Auto-Reset condition is detected, the R1 contact will remain CLOSED until all restart attempts are completed. If the fault remains after the last attempt, then the R1 contact will OPEN.

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: