Issue
Unable to connect to the G3200 gateway
Product Line
G3200
Resolution
The G3200 supports up to 6 simultaneous IEC61850 and 4 Modbus TCP/IP connections at one time. If this maximum number of connections is met, no other connections are allowed to the device.
Unable to connect to the G3200 gateway
Product Line
G3200
Resolution
The G3200 supports up to 6 simultaneous IEC61850 and 4 Modbus TCP/IP connections at one time. If this maximum number of connections is met, no other connections are allowed to the device.
Released for:Schneider Electric Nigeria