Issue
About->Support menu option missing from AP8XXX series Rack PDU Web Interface on certain firmware versions
For reference, the option should appear, as shown below:
Product Line
- Rack Power Distribution
- AP8XXX series
Environment
- All serial numbers
- Specific firmware versions - AOS v6.1.3/rpdu2g v6.0.9 APP and AOS v6.1.3/rpdu2g APP v6.1.0
Cause
This is a firmware bug.
Resolution
The firmware bug will be addressed in a future version of firmware. In the interim, this page can be accessed by manually changing the URL in the address bar.
To do this, access any web page after logging into your Rack PDU. The URL should look similar to below: http://10.10.10.10/NMC/SeCmWBB5rT0TYOwDUfIbgA/home.htm . Delete home.htm and change the URL to gentrbl.htm like this: http://10.10.10.10/NMC/SeCmWBB5rT0TYOwDUfIbgA/gentrbl.htm. Then, press enter or Go to tell your web browser to access this new URL.
Alternatively, using the CLI command logzip and downloading the debug logs from the /dbg directory via FTP or SCP still works normally as described in knowledge base article ID FA156131.
Released for:Schneider Electric Nigeria