Issue:
Why did my ATV312 run the motor in reverse when a run forward command is given?
Product Line:
ATV312
Environment:
All models
Cause:
Motor runs backwards
Resolution:
Verify the run forward command:
If using local or remote keypad command, consider the setting for CtL > rot, Rotating direction and action of the FWD/REV button.
If the correct run command is confirmed, then reverse the phasing to the motor by swapping two of the motor leads at the output of the drive, Terminals U/T1-V/T2-W/T3.
Why did my ATV312 run the motor in reverse when a run forward command is given?
Product Line:
ATV312
Environment:
All models
Cause:
Motor runs backwards
Resolution:
Verify the run forward command:
In two- wire control, LI1 is run forward.
In three- wire control, LI2 is run forward.
Monitor the logic inputs in Menu SUP > LIA- > LIS. In three- wire control, LI2 is run forward.
If using local or remote keypad command, consider the setting for CtL > rot, Rotating direction and action of the FWD/REV button.
If the correct run command is confirmed, then reverse the phasing to the motor by swapping two of the motor leads at the output of the drive, Terminals U/T1-V/T2-W/T3.
Released for:Schneider Electric Nigeria