{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do you read the color code on the IDC connectors of the Cat 6 Patch Panels?
Issue:
Customers may question which color code instructions to follow, 568B vs. 568A. Or they may not understand how to read the color code.

Product Line:
Cables and Connectivity Solutions, Cat 6 Patch Panels

Environment:
All versions and serial ranges.

Cause:
The color code instructions may be confusing.

Resolution:
For high speed networking 568B is used almost universally.
If you need help determining how to terminate to the 568B or 568A color code please see the attached file.

Schneider Electric Nigeria

Attachment(s)
20140929 T568 Color Code for Cat 6 Patch Panels.pdf [55.38 KB]
Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: