{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the mains overvoltage fault be inactivated on the ATV61 and ATV71 drives?
Issue:
Mains overvoltage fault disabling on ATV61 and ATV71 Drives

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to disable the mains overvoltage fault protection on the ATV61 and ATV71 drives.

Resolution:
It is not possible to inactivate the Mains Overvoltage detection in the drive. The trip level threshold and delay are fixed and cannot be changed.

Schneider Electric Nigeria