{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the minimum and maximum mounting depth for the SYAOPT1, and does it fit into the NetShelter 4-post rack?
Issue:
Customers may want to make sure the SYAOPT1 will mount into a particular cabinet, especially our 4-post racks.

Product Line:
Symmetra 4-Post Rack Mounting Rails SYAOPT1

Environment:
All serial ranges.

Cause:
Customers want to make sure the Symmetra 4-post rails will mount into their rack.

Resolution:

Yes, the SYAOPT1 will mount into both the NetShelter AR203A and AR204A. They are 29.42" (747mm) deep.
Minimum Mounting Depth: 27.5" (698.5mm)
Maximum Mounting Depth: 34.5" (876.3mm)

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: