Issue:
Information regarding the maximum load rating for the roof is required
Product Line:
NetShelter SX, NetShelter SV
Environment:
All versions and serial ranges.
Cause:
The load rating should not be exceeded.
Resolution:
The roofs of both the NetShelter SX and SV cabinets are rated to 200 lbs.
Information regarding the maximum load rating for the roof is required
Product Line:
NetShelter SX, NetShelter SV
Environment:
All versions and serial ranges.
Cause:
The load rating should not be exceeded.
Resolution:
The roofs of both the NetShelter SX and SV cabinets are rated to 200 lbs.
Released for:Schneider Electric Nigeria